STM32CubeMX 6.7.0 released
We are pleased to announce you that the official release of STM32CubeMX v6.7.0 is available for download here
What is new in STM32CubeMX V6.7.0?
- New CPNs: STM32WL STM32WL5MOCHx
- Boards:
- STM32WB STEVAL-PROTEUS1
- STM32F0 STM320518-EVAL
- ST32WL B-WL5M-SUBG1
- "CAD Resources" support in CubeIDE
- I-Cube "MadeForSTM32" examples description generation
- STM32L5: Cohabitation CubeAzure USBX (pack) & UCPD (MW)
- STM32F7 and STM32F4: Both ETH_RX_BUFFER_SIZE and ETH_RX_BUF_SIZE constants are specifying the size of the same buffer
- MWs upgrade:
- TouchSensing v2.2.8 for WB
- USB Device Lib v2.11.1 for L5, WB and H7
- USB Host v3.5.0 for H7
- USBPD Library v4.1.0 & device l5_v5.0.0 for L5
- USBPD Device v3.4.1 for G0
- Open Thread 1.3 for WB
- KMS v1.1.9 for WL
Main fixed issues
130537 [Project Manager] Wrong call order for MDMA/DMA Init functions
119809 [MX-L5][CodeGen] Warning generated when IP initialization as a pair of .c/.h
125698 [Cortex-M7] No default MPU configuration is proposed
126668 [MX-HRTIM][LL] Issue in HRTIM init in LL code when "General peripheral initialization as a pair of .c/.h files per peripheral " parameter is checked
128892 [IDE-GUI][H7]Changing MDMA list type from linear to loop listing causes MX tab to appear * even after saving modification
131802 [MX-CodeGen][H7] Project showing error during generation after enabling multi-threaded support checkbox for cortexM7
132093 [DMA] MX_DMA_Init() is called after MX_TIM23_Init()
133163 [STM32CubeMx] [DRR] DDR3 settings unavailable using STM32CubeMX
134921 [HRTIM] HRTIM generated code that enable Resynchronized Update even we disable it
134934 Execution in RDP-2 impacted by DWT-based code in SystemClock_Config()
135590 [MX-ETH][MW-LWIP] HAL_ETH_Start should be replaced with HAL_ETH_Start_IT in "ethernet_link_thread" function
137342 [STM32CubeMx] [FreeRtos] The tool can't open the *.ioc file if user constants are used with FreeRtos
138331 Issues with toolchain location folder and Makefile toolchain