Skip to main content
SOfne.1
Associate II
May 4, 2023
Solved

STM32CubeMX 6.8.0 and STM32CubeIDE 1.12.0: bug in initialization of GTZC, missing clock enable

  • May 4, 2023
  • 1 reply
  • 1095 views

I'm using STM32CubeIDE 1.12.0 with a TrustZone enabled project and observed incorrect initialization of GTZC when the option "Generate peripheral initialization as a pair of '.c/.h' files per peripheral" is active:


_legacyfs_online_stmicro_images_0693W00000bjNisQAE.png 

If this option is not active the function HAL_MspInit() in stm32XXXX_hal_msp.c contains some code to enable the clock of GTZC1 and/or GTZC2, depending on the further configuration e.g.:

/**
 * Initializes the Global MSP.
 */
void HAL_MspInit(void)
{
 /* USER CODE BEGIN MspInit 0 */
 
 /* USER CODE END MspInit 0 */
 
 __HAL_RCC_GTZC1_CLK_ENABLE();
 
 /* System interrupt init*/
 
 /* USER CODE BEGIN MspInit 1 */
 
 /* USER CODE END MspInit 1 */
}

If this option is active the GTZC clocks are not enabled in stm32XXXX_hal_msp.c any more. This is as expected. But the generated gtzc_s.c, which then contains the whole initialization of the GTZC, misses the code to enable the clock of GTZC1 and/or GTZC2.

Of course GTZC peripheral must be enabled (I enabled GTZC_S) in the Pinout&Configuration tab in order to trigger generation of GTZC initialization code at all.

My current workaround is to manually enable the clock(s):

/* GTZC_S init function */
void MX_GTZC_S_Init(void)
{
 
 /* USER CODE BEGIN GTZC_S_Init 0 */
 __HAL_RCC_GTZC1_CLK_ENABLE();
 /* USER CODE END GTZC_S_Init 0 */
 
 MPCBB_ConfigTypeDef MPCBB_Area_Desc = {0};
...

If you also use GTZC2 you have to add "__HAL_RCC_GTZC2_CLK_ENABLE();", too.

As far as I can see in the release notes of the latest STM32CubeMX 6.8.1, this bug has not been fixed yet.

This topic has been closed for replies.
Best answer by Ghofrane GSOURI

Hello @SOfne.1​ 

Thank you for your contributions and for your detailed explanations,

I confirm the issue on my side, it has been reported to STM32CubeMX development team .

Internal ticket number: 151261(This is an internal tracking number and is not accessible or usable by customers).

I will keep you posted with updates.

 Thx

Ghofrane

1 reply

Ghofrane GSOURI
Ghofrane GSOURIBest answer
Technical Moderator
May 4, 2023

Hello @SOfne.1​ 

Thank you for your contributions and for your detailed explanations,

I confirm the issue on my side, it has been reported to STM32CubeMX development team .

Internal ticket number: 151261(This is an internal tracking number and is not accessible or usable by customers).

I will keep you posted with updates.

 Thx

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.