Question
STM32CubeMX 6.9.2 released
STM32CubeMX 6.9.2 was released on st.com as well as an in-tool update patch.
Main issues fixed in this patch:
- Ticket 158577 - [Bootpath Config] env.bat add quotes to variable stm32tpccli
- Ticket 158868 - [Bootpath Config] secure manager post build cmd must also generate a .bin file
- Ticket 158979 - Wrong location of RAM in linker file for secure manager
- Ticket 158982 - Secure Manager : missing secure manager api files in STM32CubeIDE generation
- Ticket 159213 - Secure Manager : When enabling RTC MX does not generate SystemClock_config anymore
- Ticket 159423 - [Boot path Config] Exception occurs when changing Boot Path reference location
- Ticket 159633 - [Secure Manager] remove TPC access when "Secure Manager" Boot Path has been selected
- Ticket 160247 - Secure Manager MX code generation on MAC produce wrong postbuild.sh
Where do I obtain STM32CubeMX 6.9.2 ?
- STM32CubeMX 6.9.2: STM32CubeMX - STM32Cube initialization code generator - STMicroelectronics
- Or in the Home view click on "Check for Updates"