Skip to main content
Associate III
December 11, 2025
Solved

STM32CubeMX does NOT work in quiet mode

  • December 11, 2025
  • 1 reply
  • 887 views

Follow-on from CubeMX code generation from command line.


I am posting again in hopes of getting meaningful answer.

I tried creating a simple script text file to automate code generation for my project. The script file has all of three lines:

config load DCC_tester.ioc
generate code .
exit

The feedback I got on why it did not work was my .ico file was corrupted. To prove this was not the case I used a very simple project file using one of your example projects from one of your released STM32H5 bundles.

The only modification I made was changing the name and making it a cmake project.

I am running on Windows 11 with CubeMX installed using all defaults.

I can click on the .ioc file from Windows Explorer and the MX IDE opens just fine. I can click the "GENERATE CODE" button and that also works just fine. All the files are generated as expected.

I try launching using the -q using ether a PowerShell script or a command line batch file and neither completes although it looks like its trying.  Seems to stall leaving a MXTmpFiles folder. cmake and other files like startup and linker file are not generated.

I have attached the .ioc  the script  text file as well as PowerShell and batch file ... none work as expected.

 

Best answer by Ghofrane GSOURI

Hello @dvescovi 

Just use "exit" instead of "exit_mx"

Please remember to mark the reply that helped you as the Best Answer so that other users can more easily find this solution.

THX

Ghofrane

1 reply

Ghofrane GSOURI
Technical Moderator
December 11, 2025

Hello @dvescovi 

In your script , just do the following modification :

config load <filename>
generate code <path>
exit_mx

Example

config load "C:\Users\gsourigh\OneDrive - STMicroelectronics\Desktop\Thread\testcodegen\DCC_tester.ioc"
generate code "C:\Users\gsourigh\OneDrive - STMicroelectronics\Desktop\Thread\testcodegen"
exit_mx

 

Then launch the following command after cd the installation path of MX6.16.0 

jre\bin\java -jar .\STM32CubeMX.exe -q "script path"

example 

jre\bin\java -jar .\STM32CubeMX.exe -q "C:\Users\gsourigh\OneDrive - STMicroelectronics\Desktop\Thread\testcodegen\generatecode.txt"

As you can see , the code will be generated successfully.

GhofraneGSOURI_0-1765457590478.png

 

 

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
dvescoviAuthor
Associate III
December 11, 2025

looks like you have cubemx installed in a different location. I have mine at:

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\STM32CubeMX.exe

which is Windows standard location for everyone.

I have ioc and script in my c:/tmp/testcodegen

generatecode.txt now looks like:

config load C:\tmp\testcodegen\DCC_tester.ioc
generate code C:\tmp\testcodegen
exit_mx

launched by cd to 

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX>

then

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX>jre\bin\java -jar .\STM32CubeMX.exe -q "C:\tmp\testcodegen\generatecode.txt"

Tried again using my correct full paths and I get some source code generated but not cmake, linker startup etc.

dvescovi_0-1765481417752.png

 

dvescovi_1-1765481924636.png

you can src and inc folders and files created within but NO cmake, linker, or start up files.

 

 

dvescoviAuthor
Associate III
December 11, 2025

did not have quotes around path in generatecode.txt but even after adding them ... same results.