Associate
April 10, 2026
Solved
STM32CubeMx doesn't list STM32F767ZGT6 and STM32H743ZGT6 P2P compatible?
- April 10, 2026
- 1 reply
- 168 views
Hi,
I am trying to migrate a STM32F767ZGT6 based project to STM32H743ZGT6. According to AN4936, they should be pin to pin compatible. When I manually compared the each pin, and assigned the state of each PIN as used in STM32F767ZGT6 to STM32H743ZGT6, they seem indeed to be P2P compatible too.
But If I try to list PIN compatible MCUs in STM32CubeMx, as of the latest v6.17.0, STM32H743ZGT6 is not listed. Please see the screenshot below:

Am I missing something? Or this is a bug in CubeMX? I just don't want to throw 100s of $ down the sink. I attached my IOC file to see if anyone can reproduce my problem.
Thanks.