Skip to main content
Associate
March 31, 2024
Question

stm32cubemx for STM32H573: why is filex "mmc interface" greyed out

  • March 31, 2024
  • 1 reply
  • 951 views

I'm using the STM32H573I-DK and it works great. We are running the Fx_uSD_File_Edit example.    We are creating a product that leverages a lot of the dev kit design, but we want to use eMMC instead of SD card.  I took the Fx_uSD_File_Edit example ioc and altered SDMMC1 to be "MMC 4 bit wide bus". But now FileX does not let me choose "MMC interface".   I tried quitting out of STM32CubeMX and restarting it. No help.   I disabled SDMM1 and re-enabled "MMC 4 bit wide bus".   FileX MMC interface is still greyed out.  What can I do to change to MMC for FileX?  I've attached my .ioc

 

BTW, I have another unrelated STM32U5 project and I can choose FileX MMC interface there.  Why not in STM32H5?

This topic has been closed for replies.

1 reply

nouirakh
ST Employee
April 2, 2024

hello @billw 

I confirm the issue and it is reported internally.
Internal ticket number: 178050 (This is an internal tracking number and is not accessible or usable by customers).

With Regards
Kholdoun