Skip to main content
Explorer
March 20, 2026
Solved

STM32CubeMX Generates different names for interrupt handler in startup file & stm32l4xx_it.c

  • March 20, 2026
  • 1 reply
  • 209 views

Hi everyone,

I just started developing software for a new project containing on of the STM32L4P5 series microcontrollers. Therefore I bought the NUCELO-L4P5ZG starter-kit to get used to the IDE, HAL and so on. I use the STM32CubeMX IDE (Version 6.16.1) to configure the board and generate the basic initialization sources. Further code writing is done in STM32CubeIDE (Version: 2.1.1).

For the beginning I configured three GPIO pins for the LEDs on the board and the LPUART for simple data transfer to terminal on host computer. For the transmission I want to use DMA . After generating the code with CubeMX and implementing some simple blink logic for the LEDs, I added the line HAL_UART_Transmit_DMA(&hlpuart1, buffer, 14); to the main loop. I debugged the code and saw that the code ran into the infinite loop in the DefaultHandler in the startup file startup_stm32l4p5zgtx.s:

 

After searching for two and a half hour I finally found the problem: the generated names for the interrupt handler in the startup file and the stm32l4xx_it.c are slightly different. See the following sections:

image.png

and 

image.png

After changing the name manually in the stm32l4xx_it.c file everything works fine (until the next generation of the initialization code with CubeMX).

Please see this as a bug report and consider this issue for new releases of CubeMX.

Attached: my entire project.

Best answer by TDK

It appears this bug has been fixed. The code generates correctly on the latest STM32CubeMX version. Update your STM32CubeMX to fix this.

	.word	EXTI0_IRQHandler
	.word	EXTI1_IRQHandler
	.word	EXTI2_IRQHandler
	.word	EXTI3_IRQHandler
	.word	EXTI4_IRQHandler
	.word	DMA1_Channel1_IRQHandler
	.word	DMA1_Channel2_IRQHandler
	.word	DMA1_Channel3_IRQHandler
	.word	DMA1_Channel4_IRQHandler
	.word	DMA1_Channel5_IRQHandler
	.word	DMA1_Channel6_IRQHandler
	.word	DMA1_Channel7_IRQHandler
	.word	ADC1_2_IRQHandler
	.word	CAN1_TX_IRQHandler
	.word	CAN1_RX0_IRQHandler
	.word	CAN1_RX1_IRQHandler
	.word	CAN1_SCE_IRQHandler

 

Or, as a workaround, put

#define DMA1_Channel7_IRQHandler DMA1_CH7_IRQHandler

 in a USER CODE block at the top of the *_it.c file.

1 reply

TDK
TDKBest answer
Super User
March 20, 2026

It appears this bug has been fixed. The code generates correctly on the latest STM32CubeMX version. Update your STM32CubeMX to fix this.

	.word	EXTI0_IRQHandler
	.word	EXTI1_IRQHandler
	.word	EXTI2_IRQHandler
	.word	EXTI3_IRQHandler
	.word	EXTI4_IRQHandler
	.word	DMA1_Channel1_IRQHandler
	.word	DMA1_Channel2_IRQHandler
	.word	DMA1_Channel3_IRQHandler
	.word	DMA1_Channel4_IRQHandler
	.word	DMA1_Channel5_IRQHandler
	.word	DMA1_Channel6_IRQHandler
	.word	DMA1_Channel7_IRQHandler
	.word	ADC1_2_IRQHandler
	.word	CAN1_TX_IRQHandler
	.word	CAN1_RX0_IRQHandler
	.word	CAN1_RX1_IRQHandler
	.word	CAN1_SCE_IRQHandler

 

Or, as a workaround, put

#define DMA1_Channel7_IRQHandler DMA1_CH7_IRQHandler

 in a USER CODE block at the top of the *_it.c file.

"If you feel a post has answered your question, please click ""Accept as Solution""."