Skip to main content

4 replies

Asantos
AsantosAuthor
Associate III
May 9, 2020

Hi,

I can't enable LWIP_MDNS in MDNL/TFTP and i also can't enable LWIP_IGM in the "General Settings", of the STM32CubeMX V5.61.

why can I enable these features?

I'm trying to configure mDNS protocol for the LwIP.

I set up:

//at the end of the MX_LWIP_Init()

mdns_resp_init();

  mdns_resp_add_netif(&gnetif, "myhost", 60);

  mdns_resp_add_service(&gnetif, "myhost", "_http", DNSSD_PROTO_TCP, 80, 300, http_srv_txt, NULL);

// in fuction: static void low_level_init(struct netif *netif)

 #if LWIP_IPV4 && LWIP_IGMP

 netif->flags |= NETIF_FLAG_IGMP;

  #endif

// In LwIP options

#define LWIP_IGMP 1

#define LWIP_MDNS_RESPONDER 1

#define LWIP_NUM_NETIF_CLIENT_DATA (LWIP_MDNS_RESPONDER)

//And I include this callback function in lwip.c

static void http_srv_txt(struct mdns_service *service, void *txt_userdata)

{

  mdns_resp_add_service_txtitem(service, "path=/", 6);

}

//these function is only called once.

What am I missing?

Pavel A.
Super User
May 9, 2020

The Cube package for H7 has outdated LwIP version 2.03.

The feature you need may be in newer version 2.1x, this can be found in other packages - F7, F4...

-- pa

Asantos
AsantosAuthor
Associate III
May 10, 2020

--pa

LwIP version 2.03 also have support for mDNS. I tried to implement it using the latest STM32CubeMx for the F7, and it does not enable mDNS also .

I tested it in a MIMXRT1021 board from NXP, and there are an example of http server with mDNS, and it works well. I noticed that it depends on setting the ethernet MAC to multicast address 01 00 5E XX XX XX. I don't know how to do it on the STM32H7.

hasseb
Visitor II
December 25, 2020

"When MEMP_MEM_MALLOC is disabled, use LWIP_IGMP requires LWIP_MULTICAST_TX_OPTIONS enabled and also MEMP_NUM_IGMP_GROUP>1."

In addition, you need to have the following

MDNS_MAX_SERVICES 1

MDNS_RESP_USENETIF_EXTCALLBACK 1

LWIP_NETIF_STATUS_CALLBACK 1

LWIP_NETIF_EXT_STATUS_CALLBACK 1

You need to add following to the static void low_level_init(struct netif *netif) as well

// Allow multicast packets

ETH->MACPFR |= (1<<4);

Associate II
March 4, 2024

In case someone else struggles with this, note that LWIP_MULTICAST_TX_OPTIONS is enabled or disabled as an Advanced option within the Key Options tab.

Ergo, one must tap 'Key Options', select 'Show Advanced Parameters', and look for 'LWIP_MULTICAST_TX_OPTIONS' within the 'IPv4 - Multicast Options' tree item to enable or disable this option.

If the option is disabled, you may not be able to enable LWIP_IGMP, and that may prevent you from enabling LWIP_MDNS.