STM32CubeMX not generating syscalls.c and sysmem.c
Hi everyone,
I used STM32CubeMX (version 6.11.1) to generate the initialization code for an STM32G491RCT.
The toolchain is configured as a Makefile project.
At the end of the C_SOURCES definition, it specifies sysmem.c and syscalls.c.
# C sources
C_SOURCES = \
Core/Src/main.c \
...
Core/Src/sysmem.c \
Core/Src/syscalls.cHowever, those two files were not generated, resulting in the following error:
make: *** No rule to make target 'build/sysmem.o', needed by 'build/firmware.elf'. Stop.
Is this a bug in STM32CubeMX or am I supposed to implement the functions myself?