Skip to main content
AAnth.1
Senior
February 22, 2026
Solved

STM32CubeMX on MacOS buggy - does not show (sub)-folders

  • February 22, 2026
  • 1 reply
  • 172 views

Hi

I recently started using STM32CubeMX on MacOS and noticed that navigating through the (sub)-folder is kind of buggy or I am doing something utterly wrong.

I want to create a project inside my documents folder. But everything that is inside my documents folder is not shown in the STM32CubeMX GUI when selecting a project folder. See attached picture.

 

Can you please attempt to recreate this?

 

I use a MacBook Air M3 16GB/265GB, Mac Tahoe V26.2 should that matter.

Screenshot 2026-02-22 at 08.42.43.png

Best answer by Ghofrane GSOURI

Hello @AAnth.1 

For macOS the full disk access is required to load project files or install other packages from the file system. To enable full disk access for STM32CubeMX:
1. Go to “System preferences” and click to open “Security & Privacy” window
2. Select “Privacy” tab
3. Select “Full Disk Access” from the left panel
4. Click the checkbox to enable full disk access to STM32CubeMX

--> Hence, all folders will be visible.

This is detailed in the user manual of MX, particularly in section "3.1.1. Supported operating systems and architectures"

THX

Ghofrane

1 reply

Ghofrane GSOURI
Ghofrane GSOURIBest answer
Technical Moderator
February 23, 2026

Hello @AAnth.1 

For macOS the full disk access is required to load project files or install other packages from the file system. To enable full disk access for STM32CubeMX:
1. Go to “System preferences” and click to open “Security & Privacy” window
2. Select “Privacy” tab
3. Select “Full Disk Access” from the left panel
4. Click the checkbox to enable full disk access to STM32CubeMX

--> Hence, all folders will be visible.

This is detailed in the user manual of MX, particularly in section "3.1.1. Supported operating systems and architectures"

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.