STM32F103C8: CubeMX reports conflicts when selecting 3 UARTs plus USB
I was setting up a project which uses 3 UARTs + USB on a F103.
CubeMX reports a conflict on UART 1 when USB is configured.
I checked the ref man and datasheet but was unable to
see from what this conflict should arise.
There are no shared pins between these IPs.
I also diffed the generated code between variants with USART1
disabled or enabled and did not see obviuos diffs which do not originated
in the fact of wether USARt1 was configured or not.
Is this a false positive on CubeMXes' side?
Thanks.
#usb #cubemx-project #stm32f1-uart