STM32F7 - Unable to Select I2S Mode for SAI1 in CubeMX
Hi: My goal is to perform full-duplex I2S using the STM32F722RET6 part. To achieve this using the pins available on the package it looks like I need to use SAI2 (sub-block B) as the master/TX and SAI1 (sub-block A) as a slave/RX synchronized to SIA2.
The configuration of SIA2 in CubeMX works fine. However, when I attempt to configure the slave side (SAI1-A) the I2S option is greyed out (see below). Can anyone help me to debug this? Many thanks, Bruce.