Skip to main content
tinkerer42
Associate III
August 27, 2024
Question

STM32G473 ADC - can't select asynchronous clock divider 1 or 2, even with low clock frequency

  • August 27, 2024
  • 1 reply
  • 901 views

Hi,

I'm using STM32G473 ADC and trying to feed its clock from the PLL P clock. I am not able to select a clock divider of 1 or 2 even when the PLL P clock is set rather low (11.2 Mhz). This is my clock configuration:

tinkerer42_1-1724716914794.png

 

This shows CubeMx not allowing an async clock with divider of 1 or 2, only 4 and higher:

tinkerer42_2-1724717026384.png

 

For reference, these are the frequency limits of the ADC from the datasheet:

tinkerer42_3-1724717178333.png

Specifically, I'm at the 52 MHz max spec (single ended, multiple ADC's) but whatever CubeMX thinks my limit is, I'm not sure why I can't divide-by-1 a 11.2MHz clock!

 

Is this a bug and I should use manual lines of code overriding what CubeMX does? or am I missing something in my understanding of the ADC clock?

p.s. my goal is to get as close to my limit of 52 MHz as possible. The 11.2 MHz setting shown above was just to debug CubeMX's weird behavior.

 

Thanks!

 

1 reply

tinkerer42
Associate III
August 27, 2024

OK, I fiddled with the settings some more and discovered another thing: If I enable only ADC1 and ADC2 (or just ADC1) then I can select my prescaler as expected. However, if I enable ADC3 as well, then I can't select /1 or /2, only /4 or higher, as noted in my original post.

I can't find a reference to this limit in the datasheet. Why is that?