Skip to main content
HMüll.4
Senior
June 18, 2025
Solved

STM32H735G-DK: RGMII Ethernet interface with RX_ERR?

  • June 18, 2025
  • 2 replies
  • 555 views

Hi,

when looking into the schematics of the STM32H735G-DK board (MB1520B), the Ethernet-PHY is connected via RMII.

Now when I configure RMII for an STM32H7 in CubeMX, the interface pins do fit properly to what is used in the MB1520B schematics - except the RX_ERR-line. According to the schematics it is connected to PB10, but when I enable PB10 in CubeMX for use as RX_ERR, it is marked in yellow with the remark "no mode".

So...how do fit both things together? How can I enable RX_ERR being used in Cube MX for RMII-mode?

Thanks!

 

Best answer by LCE

Not an error! You could still set the GPIO to interrupt mode, or poll it.

Anyway, Cube is not perfect...

Edit: found it in the datasheet!

But the H7 ETH-peripheral's RMII doesn't do anything with that pin, except that it sets a bit in an RX descriptor.

Still not sure if that's the case for MII or RMII, in the datasheet it's called only " MII_RX_ER ", all RMII signals are usually called " RMII_* ".

Is the signal connected to the PHY ?

2 replies

LCE
Principal II
June 18, 2025

Check the datasheet for the alternate functions, I faintly remember that RX_ERR is simply not supported by the H7 hardware. But I might be wrong.

And it's definitely RMII, without the "G". ;)

HMüll.4
HMüll.4Author
Senior
June 24, 2025

So this would be an error in the evaluation board from ST then!?

LCE
LCEBest answer
Principal II
June 24, 2025

Not an error! You could still set the GPIO to interrupt mode, or poll it.

Anyway, Cube is not perfect...

Edit: found it in the datasheet!

But the H7 ETH-peripheral's RMII doesn't do anything with that pin, except that it sets a bit in an RX descriptor.

Still not sure if that's the case for MII or RMII, in the datasheet it's called only " MII_RX_ER ", all RMII signals are usually called " RMII_* ".

Is the signal connected to the PHY ?