Skip to main content
Roger.ch
Associate III
April 18, 2023
Question

STM32H750XBH6 Data Flash Memory for Application Data.

  • April 18, 2023
  • 2 replies
  • 1169 views

Does the STM32H750XBH6 have data flash memory that I can use to store 200 bytes of application data? For example to store the IP address etc.. 

The datasheet says something about "2 Kbytes (64 flash words) of user option bytes for user configuration". Is there a driver from ST for this memory? How do I activate this driver in MXCube?

Best regards Roger

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
April 18, 2023

There should be FLASH (OTP, Option Byte) examples in the CubeH7 board example forks.

Check also API descriptions/syntax in HAL stm32h7xx_flash.c and flash_ex.c type files

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
Pavel A.
Super User
April 18, 2023

STM32H7 does not have OTP.

AFAIK there is no public reliable way to use the "option bytes" space.

It is possible to write these 200 bytes into free space after the end of the firmware (as usual - aligned on 32 bytes..)