Skip to main content
Associate II
April 16, 2025
Solved

Support relative paths when targetting MDK-ARM toolchain

  • April 16, 2025
  • 1 reply
  • 573 views

Using "Firmware Relative Path" currently have 2 problems:

  • The path in the text field is displayed as absolute while the actual path is stored in the .ioc file as relative
    • This is somewhat confusing to the user as CubeMX will display different (absolute paths) for different users with the same .ioc file.
  • Targetting the MDK-ARM toolchain will generate/update an .uvprojx file with absolute paths and not relative paths
    • This is an issue when the firmware is stored in a vcs repository and share among several developpers which don't have their local copy at the same location. For each developper re-generating code with CubeMX, absolute paths on its computer will be appended in the Keil file. Therefore we need to manually remove them in the .uvprojx file before commiting our changes to the repository.

Would it be possible to use relative paths instead (or support them alongside absolute paths) in CubeMX and uVision project file ? Looking at other posts in the community, it seems CubeIDE has the same issue.

 

Best answer by Ghofrane GSOURI

Hello @vchatelain 

A change request has been raised to dev team for feasibility check.

Internal ticket number  205362 

I will keep you posted with updates.

THX

Ghofrane 

1 reply

Ghofrane GSOURI
Ghofrane GSOURIBest answer
Technical Moderator
April 16, 2025

Hello @vchatelain 

A change request has been raised to dev team for feasibility check.

Internal ticket number  205362 

I will keep you posted with updates.

THX

Ghofrane 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
April 16, 2025

Thank you for the quick response !