The chip text orientation in STM32CubeMX/MX2 does not match reality. Why?
In STM32CubeMX, here is the orientation for a chip with a red dot marking pin 1 at the top left when text reads from left to right.

In real life, here is the orientation for a chip with a red dot marking pin 1. As far as I'm aware, all STM32 chips are oriented like this, with pin 1 at the bottom left when text reads from left to right.

Why is the text rotated 90 degrees differently? Is this intentional? If there is a reasonable explanation, I'm interested in hearing it. It seems to only add confusion. Wouldn't it make more sense if the default orientation (or at least the text orientation) to match between the two?
In STM32CubeMX, you can rotate the part for convenience. This is useful. However, the text also rotates, so if you put pin 1 in the bottom left like in reality, the text is now rotated.

(This is the same story in STM32CubeMX2.)