Skip to main content
Associate II
October 11, 2024
Solved

To Generate 2 pwm with phase shift with same timers

  • October 11, 2024
  • 1 reply
  • 1559 views

1000012502.jpg

logic analyser picture has timer 1 channel 1 and another one is channel 2 it's duty 30% and frequency 100khz it's total ton+toff is 10 microseconds here I need to start the timer 1 channel 2 after 5 microseconds  I need the output like this I I'm drawn here

1000012503.jpg

im using STM32H743IGT6 I had got the output in 50% duty but I can't get output other than 50% duty please help me anyone.

Best answer by AScha.3

>combined mode but that didn't work 

So you set it wrong .

read rm:

AScha3_0-1728640257525.png

 

1 reply

waclawek.jan
Super User
October 11, 2024

Use the Combined PWM mode.

JW

Associate II
October 11, 2024

How can I do that I'm change pwm as combined mode but that didn't work 

AScha.3
AScha.3Best answer
Super User
October 11, 2024

>combined mode but that didn't work 

So you set it wrong .

read rm:

AScha3_0-1728640257525.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."