Trouble Installing STM32CubeMX 6.15.0 on Windows 11 (64bit)
Hello Forum,
I am trying to install STM32CubeMX version 6.15.0 on Windows 11 (64bit). I want to install it for "all users". I've downloaded and extracted the archive. I can run the installer 'SetupSTM32CubeMX-6.15.0-Win.exe' with Admin privileges and it extracts and runs to the "Select Install Mode". At this point if I choose "Install for all users" then the dialog just exits and nothing happens. It works as expected with STM32CubeMX version 6.12.0
Does anyone have any ideas on what's going wrong? A big ask I know. Can anyone suggest where to look for clues, are there any install logs that may give me a clue as to what's happening?
Here are the machine details:
- Windows Type: Windows 11 Enterprise, Version 24H2, OSBuild 26100.4946
- Processor: 13th Gen Intel(R) Core(TM) i5-1335U (1.30 GHz)
- RAM: 64.0 GB (63.6 GB usable)
- System Type: 64-bit operating system, x64-based processor
- Disk: 477GB free space on the SSD, C:\
Update: I've also tried this on a separate Windows 11 (64bit) machine and see the same issue.
Any help appreciated,
DD