Question
Unknown confilct in CubeMX for RTC calibration output on STM32H7R7
If I activate the calibration output 1 of the RTC, CubeMx lags and afterwards marks the options red with "unkown conflict". GPIO does not get assigned or gets cleared if done manually before. Same behavior for 1Hz and 512Hz output. OUT2 works.
restarted application and PC, still the same
uC: STM32H7R7L8H6H
CubeMX V6.13.0
FW versions see below


Thanks and regards