Skip to main content
Associate
November 28, 2023
Question

Usage of this same ADC pin on two ADC instances

  • November 28, 2023
  • 3 replies
  • 2427 views

Hello, I am working on STM32F7x uC and I want to use one GPIO pin, e.g. PA3 as analog input. However, value from analog input should be read both by ADC1 and ADC2. CubeMX allows me that configuration and it should work. However, when I deinitialize only ADC1 then ADC2 stops work too. The reason is fact that generated: HAL_ADC_MspDeInit() function just deinitializes PA3 pin and it does not take into account that the other instance of ADC uses this pin as well.

is it kind of limitation of CubeMX solution? or Do I miss something else and there is a limitation of hardware and one GPIO pin cannot be used by two (or more) instances of ADC simultaneously?

Best regards and thanks in advance for any tips.

 

 

 

 

This topic has been closed for replies.

3 replies

ST Employee
November 28, 2023

Hello @Tomnow1

>>here is a limitation of hardware and one GPIO pin cannot be used by two (or more) instances of ADC simultaneously

It is possibleto use two ADCs with the same pin as an analog input: IO is in analog mode and shared (not alternate function)

If you're using more than one ADC instance, you might want to modify the generated HAL_ADC_MspDeInit() code to avoid calling __HAL_RCC_ADC_CLK_DISABLE, or at least be aware that all ADCs use the same clock and disabling the clock will reset all ADCs. so this is quite predictable... 

 

Technical Moderator
November 28, 2023

Hello @Tomnow1,

No HW limitation, but probably a feature still not covered by CubeMx.

For this example as workaround, you might comment call to HAL_GPIO_DeInit(GPIOA, GPIO_PIN_3); in HAL_ADC_MspDeInit() function in order to avoid "deinitialize the GPIOx peripheral registers to their default reset values."

 

Best regards

Tomnow1Author
Associate
December 6, 2023

Hello, thanks for your feedback. It's clear to me that I can handle it myself by modifying generated code. Thank you to make me sure about that.

--

Best regards