Skip to main content
Associate III
October 3, 2024
Solved

Usart 3 not a available on NUCLEO H755ZIQ in CubeMx

  • October 3, 2024
  • 1 reply
  • 912 views

Good morning , I have a problem on stm32: USART3 is impossible to put  into available:

Jad_0-1727964328756.png

 

the schematics of my nucleo 144 tell me however to use usart 3: 

IMG_9603.jpeg

I wanted to do it manually by turning directly the pins of PD9 and PD10 into tx nd rx but it doesn't want to turn on the usart3. I think I am missing something.

 

Best answer by mƎALLEm

Hello,

How did you start your project in CubeMx? from MCU part number or from Nucleo board?

If it was from the board, USART is already configured for you when you selected to initialize the peripherals

SofLit_1-1727965341247.png

 

SofLit_0-1727965221824.png

PS: UART3 Tx/Rx are on PD8 and PD9 not on PD10.

1 reply

mƎALLEm
mƎALLEmBest answer
Technical Moderator
October 3, 2024

Hello,

How did you start your project in CubeMx? from MCU part number or from Nucleo board?

If it was from the board, USART is already configured for you when you selected to initialize the peripherals

SofLit_1-1727965341247.png

 

SofLit_0-1727965221824.png

PS: UART3 Tx/Rx are on PD8 and PD9 not on PD10.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
JadAuthor
Associate III
October 3, 2024

I started it directly on IDE from nucleo.i begin from IDE since it has the gui of cubeMX now.