Why are there random breakpoints in the assembly code and how to get rid of them?
I'm migrating a project from STM32G431KB to STM32G431CBT6. Both projects were generated using STM32CubeMX and are developed in Keil (MDK ARM), so I only transferred the user code. However when debugging code on the new chip, random breakpoint commands in the disassembly window appear (not the user-defined red dots, but the BKPT mnemonic specifically).
It's always first 3 times between _sys_open and _sys_close, then one time between _sys_istty and_sys_seek and another one between _sys_write, _sys_read, then my program runs normally. I tried a full chip wipe, code regeneration, code rebuilds all without any luck. I'm guessing there might be a setting I forgot somewhere that could cause this or a library from CubeMX, but so far I haven't been able to figure out what it could be.
The CubeMX software packs I use:
Selected features: