Why does STMCube MX limit the STM32H743ZI2 Nucleo board to 300MHz max MCU Frequency
Hi There,
I'm trying to use the STM32H743Zi2 nucleo board for test purpose.
I configured the board with default settings ( when asked by CubeMX after selecting the board for a project). Means i basically did nothing (except assigning 1 ADC ppin and leaveing the rest untouched). I then tryed to configurate the Clock to use the 480MHz advertised in the datasheet, but Cube MX seems to be willing to accept only CPU Clocks below or equal to 300MHz.
- There seem to be a rounding problem while setting up the PLL values, as in the ioc file they appear to come out with decimal values that don't exist.
- main problem is still that even if setting values way below the 480MHz, CubeMX doesn't accept anything above 300MHz ( according to the hint given while hovering the error with the mouse)
I had that problem once with another board, and had no other choice than restarting the project from the scratch, but that didn't work out that time.
Cube MX is up to date(v6.7.0), and MCU Package also ( v1.11.0 for H7 MCU).
I didn't notice anything in the datasheet that would reduce drastically the maxoperation
speed of the device, but i might be wrong.
Is that a bug related to this specific MCU Package or is there something i missed here? Is there a work around to that Problem?
What happens if I generate the project with the errors still active, is there a correction/limitation somehow during the generation or are they configured so anyway?