Skip to main content
DMAYE.1
Associate II
February 10, 2021
Solved

Why would cube IDE not generate code for a free and available GPIO pin

  • February 10, 2021
  • 5 replies
  • 2681 views

The GPIO clock is the only code that seemed to be generated under the initialization function. the other necessary code such as the following was not created.

GPIO_InitTypeDef GPIO_InitStruct;

GPIO_InitStruct.Pin = GPIO_PIN_8;

GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

In the setup GUI I had selected the pin PC8, and set it to a GPIO_Output yet the above code was not generated.

Best answer by Khouloud ZEMMELI

Hi @DMAYE.1​ ,

Thanks for the share of your ioc file which allowed me to know the main reason of the GPIO configuration code disappearance.

In fact, in the case of the stm32H7 Dual Core , when the pin is not linked to an IP that we have already started its activation by choosing on which cortex it is assigned, this pin remains free, i.e, it does not know on which cortex it is up to.

For its configuration to be correctly generated, you have to choose the cortex of this pin by right click on the pin, click on the Pin Reservation and then check one of the two cortex.

Once you generate your project, you will find the complete GPIO code in the /*Configure GPIO pin : PC8 */ section under main.c/MX_GPIO_Init function :) .

0693W000008G18ZQAS.png 

Hope my answer helped you, when your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thanks for your contribution, Khouloud

5 replies

KnarfB
Super User
February 10, 2021

Never seen before. What tool / version ? What chip?

DMAYE.1
DMAYE.1Author
Associate II
February 11, 2021

stm32 cube IDE

latest version I think 1.5.1

Nucleo-144 STM32H755ZI-Q

Khouloud ZEMMELI
ST Employee
February 11, 2021

Hello @DMAYE.1​ 

Thanks for your feedback,

Could you please share your ioc file to check your problem?

Thanks, Khouloud

DMAYE.1
DMAYE.1Author
Associate II
February 12, 2021

Yes, and Thank you in advance! the .ioc file is attached.

Khouloud ZEMMELI
Khouloud ZEMMELIBest answer
ST Employee
February 12, 2021

Hi @DMAYE.1​ ,

Thanks for the share of your ioc file which allowed me to know the main reason of the GPIO configuration code disappearance.

In fact, in the case of the stm32H7 Dual Core , when the pin is not linked to an IP that we have already started its activation by choosing on which cortex it is assigned, this pin remains free, i.e, it does not know on which cortex it is up to.

For its configuration to be correctly generated, you have to choose the cortex of this pin by right click on the pin, click on the Pin Reservation and then check one of the two cortex.

Once you generate your project, you will find the complete GPIO code in the /*Configure GPIO pin : PC8 */ section under main.c/MX_GPIO_Init function :) .

0693W000008G18ZQAS.png 

Hope my answer helped you, when your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thanks for your contribution, Khouloud

Associate
April 6, 2025

Hello

I have the same issue (GPIO pin initialization to specified mode isn`t generated)
I can`t find ''pin reservation'' in pop-up from right click on pin or in any tab (pinout & configuration -> gpio mode configuration)

It`s dual-core project for stm32wl55jcix, STM32CubeMX version 6.13.0 (linux)

DMAYE.1
DMAYE.1Author
Associate II
February 12, 2021

Thank you so much. That is the issue. I was looking for the pin assignment under the system gpio tabs. It wasn't in that setup. And I think it should be. Thank you once again.​

Khouloud ZEMMELI
ST Employee
February 15, 2021

Always welcome @DMAYE.1​  :)

Khouloud