Feature Request: Multi-Profile GPIO & Peripheral Configuration for Power Mode Transitions
Hello ST Community,
I am working on an ultra-low-power project using STM32 MCUs and I have a question regarding the current capabilities of STM32CubeMX.
Current Situation: I am aware that STM32CubeMX has an option to "Set unused pins to Analog" to save power. However, this is not sufficient for complex low-power management. In many cases, pins that are actively used in "Run" mode need to be reconfigured into specific states—not necessarily Analog—before entering a low-power mode (e.g., keeping a specific Pull-up/Pull-down for an external sensor, or maintaining a specific Output level to prevent leakage through external circuitry).
Currently, CubeMX generates a single initialization function (e.g., MX_GPIO_Init()). To manage transitions for these "used" pins, we must manually write wrapper functions to change their states before sleep and re-initialize them upon wake-up. This manual process is time-consuming and prone to configuration errors.
My Question: Is there an existing feature or workflow within CubeMX that allows users to define two or more different configuration sets for the same pins/peripherals and generate separate initialization functions for them?
Feature Suggestion: If this is not currently supported, I believe it would be a massive improvement for the STM32 ecosystem. Ideally, CubeMX could have a "Mode Manager" tab where:
- Users can define custom modes (e.g., Run_Mode, UltraLowPower_Mode).
- For each mode, the user can visually set GPIO states (Analog, Pull-up, Output levels, etc.) and peripheral states for all pins, not just the unused ones.
- CubeMX generates distinct functions like MX_GPIO_Init_Run() and MX_GPIO_Init_LowPower().
This would significantly reduce boilerplate code, prevent hardware-related leakage errors during manual transitions, and make power optimization much more intuitive.
I would love to hear if there are any workarounds or if this is something the dev team might consider for future releases.
Best regards,