Skip to main content
Associate II
March 25, 2024
Solved

Motor Profiler - Motor Won't Spin - (from MC Workbench 6.2.0)

  • March 25, 2024
  • 2 replies
  • 1625 views

Hi,

This is my first post on the forum so my apologies if I’m doing something wrong.

OS:

Windows 10 64-bit

Software:

STM32CubeIDE 1.14.1

Motor Control Workbench 6.2.0

ST Motor Pilot v1.2.4

Hardware:

Dev Kit:                      P-NUCLEO-IHM002

Control Board:            NUCLEO-F302R8

MCU:                          STM32F302R8

Power Board:              X-NUCLEO-IHM07M1

Motor:                         Bull Running BR2804-1700kv

 

Problem Description:

The motor does not spin when I run the profiler using Motor Pilot v1.2.4. I can see the motor momentary jerks but it doesn’t spin and consequently the profiler fails. I have followed the profiler setup in ST Motor Pilot v1.2.4 > Help > Profiler Documentation. The profiler firmware is generated. I have compiled and uploaded the generated code with STM32CubeIDE 1.14.1. No errors or warnings are generated. When I start the profiler it hangs at 28% - the motor never rotates. See attached screenshots

In contrast I have no problems when using the Motor Pilot instead of the Motor Profiler. With the Motor Pilot the motor spins and I can adjust the speed from the GUI.

Questions:

  1. What is the problem stopping the Motor Profiler from working?
  2. How do I fix this problem?
  3. It appears that the code generated for the Motor Profiler (tick the "Motor Profiler" feature into the "Application configuration") does not work with the Motor Pilot – and code generated for the Motor Pilot does not work with the Motor Profiler. Is this correct? I didn’t see this mentioned in the documentation.

Thanks:

If anyone from ST sees this message then I want to say a sincere thank you to ST for providing all the excellent tools, software and documentation – for free! A very intelligent business decision and I’m grateful.

 

This topic has been closed for replies.
Best answer by Gael A

Hello Gary_Baldy,

I don't know if this is your case, but it feels like you generated a project with MCSDK 6.2.0, then opened the same project with MCSDK 6.2.1 and re-generated that project into the same folder without changing its name. Am I right ?
In any case, please refrain from doing this, as it generally causes a few issues. Please create a new project or save your project in a different folder / with a different name to ensure a correct generation. If the issue persists, please make sure your CubeMx, CubeIDE and Firmware package are up to date. I generated your project using MCSDK 6.2.1, CubeMX v6.11.0, CubeIDE v.1.13.2 and Firmware package v1.11.4 and had no issue.

2 replies

GMA
Technical Moderator
March 28, 2024

Hello @Gary_Baldy,

Firstly, thank you for your message.
There is a known issue on WorkBench 6.2 profiler (profiler functional for STM32G4 series only), could you please try with 6.2.1 version?

Associate II
March 31, 2024

Many thanks for your reply!

I installed 6.2.1 and re-generated the code (using the project attached to my first post). When I compiled the new code I got many errors as shown below so cannot test the profiler. Most seem to state 'undefined reference'. I've tried to solve this but haven't succeeded.

Can you help?

 

13:33:30 **** Build of configuration Debug for project motor_test_2 ****

make -j4 all

arm-none-eabi-gcc -o "motor_test_2.elf" @"objects.list" -mcpu=cortex-m4 -T"C:\Users\user\.st_workbench\projects\motor_test_2\STM32CubeIDE\STM32F302R8TX_FLASH.ld" --specs=nosys.specs -Wl,-Map="motor_test_2.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group

C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Application/User/mc_api.o: in function `MC_ProfilerCommand':

C:/Users/user/.st_workbench/projects/motor_test_2/Src/mc_api.c:716: undefined reference to `SCC_CMD'

C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Application/User/mc_tasks.o: in function `MCboot':

C:/Users/user/.st_workbench/projects/motor_test_2/Src/mc_tasks.c:890: undefined reference to `SCC_CheckOC_RL'

 

..... lines removed here due to 20,000 character limit

 

C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Application/User/register_interface.o: in function `RI_SetRegisterMotor1':

C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:559: undefined reference to `OTT_SetSpeedRegulatorBandwidth'

C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:411: undefined reference to `SCC_SetUnderVoltageThreshold'

C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:585: undefined reference to `SCC_SetResistorOffset'

C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:238: undefined reference to `SCC_SetPBCharacterization'

C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:572: undefined reference to `SCC_SetNominalSpeed'

C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:220: undefined reference to `SCC_SetPolesPairs'

C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:1398: undefined reference to `SCC_GetLdLqRatio'

C:/ST/STM32CubeIDE_1.10.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.100.202309141235/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/user/.st_workbench/projects/motor_test_2/Src/register_interface.c:1420: undefined reference to `OTT_GetJ'

collect2.exe: error: ld returned 1 exit status

make: *** [makefile:66: motor_test_2.elf] Error 1

"make -j4 all" terminated with exit code 2. Build might be incomplete.

 

13:33:32 Build Failed. 55 errors, 0 warnings. (took 1s.624ms)

 

 

Gael A
Gael ABest answer
ST Employee
April 3, 2024

Hello Gary_Baldy,

I don't know if this is your case, but it feels like you generated a project with MCSDK 6.2.0, then opened the same project with MCSDK 6.2.1 and re-generated that project into the same folder without changing its name. Am I right ?
In any case, please refrain from doing this, as it generally causes a few issues. Please create a new project or save your project in a different folder / with a different name to ensure a correct generation. If the issue persists, please make sure your CubeMx, CubeIDE and Firmware package are up to date. I generated your project using MCSDK 6.2.1, CubeMX v6.11.0, CubeIDE v.1.13.2 and Firmware package v1.11.4 and had no issue.

Associate II
April 3, 2024

Yes, you are correct I opened an existing 6.2.0 project in 6.2.1 and re-built it.

I followed your advice, updated all software components and created a new MC project and now the profiler works.

Many thanks for your assistance!