STM32WL55 FSK receive bandwith setting, SubGHz_Phy_Per example
Hi,
the STM32WL55's reference manual states:
> BW[DSB] > BR + 2 x frequency deviation + frequency error
However, in the SubGHz_Phy_Per example, FSK is configured as follows:
#define FSK_FDEV 25000 /* Hz */
#define FSK_DATARATE 50000 /* bps */
#define FSK_BANDWIDTH 50000 /* Hz */
Therefore, "BR + 2 x frequency deviation" would be equal to 100000Hz. But the bandwidth is set to just 50000Hz. But the example still works. Why? The gaussian filter (BT=0.5) reduces the bandwith, but not that much.
The reference manual also states:
> In receive mode, the bandwidth is automatically adjusted to match the selected data rate
Does this mean I don't have to specify the bandwidth?
Is the following interpretation of the FSK frequency parameters correct?