cannot launch UserAPP after SBSFU
Hi, I am a beginner in SBSFU.
STM32L4S7ZIT6
STM32CUBEIDE Version: 1.12.0
STM32CUBEProgrammer v 2.13.0 (for download SBSFU and full chip erase)
Tera Term v 4.106
When run SBSFU, I can get EXECUTE USER FIRMWARE at end, but cannot run UserAPP.

if reset SBSFU, still cannot run UserAPP.

I have done some debug:
1. never use RDP2 level 2
2. boot is set to GND
3. modify linker_common and STM32L4S7ZITX_FLASH.ld by STM32CubeExpansion_SBSFU_V2.6.2 (B-L4S5I-IOT01A)

4. modify system_stm32l4xx.c and STM32L4S7ZITX_FLASH.ld in UserAPP for SBSFU( if don't change, i mean that UserAPP can run normally without SBSFU)
5. disable SECBOOT_DISABLE_SECURITY_IPS at app_sfu.h
reference:
1. if i run UserAPP alone, it show error Break at address "0x1fff51da" with no debug information available, or outside of program code. then it can run to main.

2. if i run SBSFU alone, it show error Break at address "0x1fff51da" with no debug information available, or outside of program code. then it can run to main. (i think the correct one is i can see run at startup_stm32l4s7.s then back to main)

i don't know why after SBSFU the UserAPP cannot run. Maybe the point is 0x1fff51da?
it will be very helpful, if any one tell me something.
thank you.