Associate II
January 24, 2025
Solved
Adding breakpoint and debugging using UDE STK 2021
- January 24, 2025
- 1 reply
- 2966 views
Hello everyone,
I have been flashing the code written in AutDevKit Studio 2.4.0 using UDE STK 2021 for the AEK-AUD-C1D9031, which uses the SPC582B60E1 MCU. I want to start debugging the code line by line using breakpoints.
Currently, I have the option to add breakpoints in AutDevKit Studio, but it is of no use since I am flashing the code with UDE STK 2021.
Could someone guide me on how to add breakpoints in UDE STK 2021? Also, how can I add variables to the watch window?
I referred to the manual I attached but couldn’t figure out the exact steps to add breakpoints or watch variables in the program shown in UDE STK 2021.