Skip to main content
Associate II
December 5, 2025
Solved

Availability of High-Level BMS APIs (AEK_POW_BMS63EN) in AutoDevKit

  • December 5, 2025
  • 1 reply
  • 377 views

Hello,

In the AEK-POW-BMSCHAIN example code, I see high-level APIs like:

 
AEK_POW_BMS63EN_GetModule() AEK_POW_BMS63EN_init()

But in my AutoDevKit installation, only low-level chain APIs (AEK_POW_BMS63CHAIN_*) are available.

Could you clarify:

  1. Are the high-level AEK_POW_BMS63EN APIs included in the public AutoDevKit package?

  2. If not, are they only available via partner/NDA packages?

  3. Should regular users implement high-level functionality using only the low-level APIs?

Thanks!

Best answer by Max VIZZINI

Hi,

No, there is no reserved code / package.

The code is available for evaluation purposes.

If you need design support to your coding, you can consult with our partner https://www.beond.net/electronics/ 

Best Regards,

AutoDevKit Team

1 reply

Max VIZZINI
Max VIZZINIBest answer
Technical Moderator
December 6, 2025

Hi,

No, there is no reserved code / package.

The code is available for evaluation purposes.

If you need design support to your coding, you can consult with our partner https://www.beond.net/electronics/ 

Best Regards,

AutoDevKit Team