Skip to main content
Associate II
January 29, 2025
Solved

BMS63EN 14 Cell GUI

  • January 29, 2025
  • 2 replies
  • 1183 views

Hello,

I am trying to set up the 14 cell GUI using the C4MLIT1, ISOSPI1, and BMS63EN boards. At this point in time, I am only interested in the logging functionality and just want to use the demo as it comes.

I have the hardware set up in centralized configuration, with just a single BMS63EN connected to 14 cells via the BMSHOLD cell holder (~56 V total). When I start the GUI, the serial port connects, but no data appears.

Could someone advise on whether I have understood the broad steps correctly, starting from having AutoDevKitStudio installed and GUI project imported?

  1. Move GUI .exe to desktop.
  2. Connect ISOSPI1 to MCU as per the board view schematic, shown by clicking "SPC58EC 4M board view". Also connecting vcc and vio to 5V.
  3. Connect BMS63EN to ISO board via USB connector.
  4. Connect BMSHOLD cell holder (with cells) to BMS63EN
  5. Connect MCU to PC and generate + compile
  6. Start GUI

I just want to confirm whether I have the simple stuff right first before moving on. I'm slightly concerned I may have burnt the chip. How can I diagnose whether the issue is with the SPI <> MCU board connections, or with the BMS <> SPI board connections?

For info, the only LEDs illuminated on the ISOSPI1 are FAULT and D7. On the BMS63EN, D2 briefly flashes on when the cells are connected, but then turns off and stays off.

Best answer by SRomeo

Hi Luke,
Make sure the connection between ISOSPI USB and BMS63EN is performed using the ISOL port of your BMS63EN.

It is crucial to perform the flashing procedure in between step 5 and 6.So, if all other steps were executed correctly, I think you are missing to "install" the compiled code on your C4MLIT1. 

Here attached you can find the detailed description on how to install compiled code on an AEK MCU board.

  •  Start from slide 1 if you are missing OpenOCD Drivers.
  •  else, Start from slide 7 

    I hope this helps,
    SR,
    AEK Team

2 replies

SRomeo
SRomeoBest answer
ST Employee
January 30, 2025

Hi Luke,
Make sure the connection between ISOSPI USB and BMS63EN is performed using the ISOL port of your BMS63EN.

It is crucial to perform the flashing procedure in between step 5 and 6.So, if all other steps were executed correctly, I think you are missing to "install" the compiled code on your C4MLIT1. 

Here attached you can find the detailed description on how to install compiled code on an AEK MCU board.

  •  Start from slide 1 if you are missing OpenOCD Drivers.
  •  else, Start from slide 7 

    I hope this helps,
    SR,
    AEK Team
Luke_AAuthor
Associate II
February 11, 2025

Thanks very much, that's solved my issue. I have a separate query relating to the chain demo using the same hardware but will raise that in a new thread. Thanks again!