Debugging with AEK-MCU-SPC5LNK but no debugging information showed
Hi,
I am working with an AEK-MCU-C4MLIT1, and trying to debug using the debugger AEK-MCU-SPC5LNKA through the JTAG port. I did a very simple code because all I am interested in now is to ensure that the debugger works properly. The debugging session seems to start properly, as no errors or interruptions occur during the starting phase. The problem is that "Peripherals" and "Memory" are complitely empty while the debug session is running. At the beginning of every debug session the following message shows up: "Break at address "0x404100" with no debug information available, or outside of program code." May it be related to the problem I am encountering?. What I could do?
Thanks.