Skip to main content
Associate III
April 22, 2024
Solved

struck in wait_for_transfer_completion() when I enable freeRTOS. for AEK_AUD_C1D9031.

  • April 22, 2024
  • 1 reply
  • 655 views

shiva_shankar_e_0-1713787970729.png

I debug up to hear and the flow of the code is blocked in this function,(after adding freeRTOS) in  the project. i don't know what is the error. i had used the low level API which is avaliable in the document. 

shiva_shankar_e_1-1713788885119.png

the flow is like this in the main function. at AEK_903D_Init(). it is blocked. and not coming out of that API. please help me out.

Best answer by Max VIZZINI

Hi,

As I have already stated, the code has NOT be written from freeRTOS therefore it requires modification.

In particular all osalThreadDelay() are not working under freeRTOS. They have to be substituted with:

 

vTaskDelay () specifies a wake time relative to the time at which the function is called

OR

vTaskDelayUntil () specifies the absolute (exact) time at which it wishes to unblock

 

Example code:

TickType_t xLastWakeTime = xTaskGetTickCount();

vTaskDelayUntil( &xLastWakeTime, 200 );

where 200 are in milliseconds.

 

Best Regards,

AutoDevKit Team

1 reply

Max VIZZINI
Max VIZZINIBest answer
Technical Moderator
April 22, 2024

Hi,

As I have already stated, the code has NOT be written from freeRTOS therefore it requires modification.

In particular all osalThreadDelay() are not working under freeRTOS. They have to be substituted with:

 

vTaskDelay () specifies a wake time relative to the time at which the function is called

OR

vTaskDelayUntil () specifies the absolute (exact) time at which it wishes to unblock

 

Example code:

TickType_t xLastWakeTime = xTaskGetTickCount();

vTaskDelayUntil( &xLastWakeTime, 200 );

where 200 are in milliseconds.

 

Best Regards,

AutoDevKit Team