Issue with UDESTK Connection with L9963E BMS board I have a L9963E BMS development board, I have tried connecting to SPC5 UDESTK Debugger, the debugger is not getting connected (UDE STK Debugger) to the controller I have connected the power adapter and USB mini connector as well, I am using UDESTK Staterkit 2021 version from pls. The error indicates No Target Supply or JTAG Cable Connection or Target ConfigurationTargetConfiguration I have selected from the provided list Power to the board is proper I have connected the adapter and to rule out if it is taking power from USB of Serial cable, I have connected the serial cable i.e., the FTDI cable as wellToConfirm the power to the board is fine, I have ran the default firmware whichis shipped along with the board, it is getting connected to theL9963_evaluation_GUI program and serial communication is OK. how can we connect the debugger, any settings needed in the development board to be done or any jumper settings need to be changed?AlsoIs there a facility to connect t