About LSM330DLC Gyroscopes reflow solder problem
We used
LSM330DLC Gyroscopes in electric self-balancing unicycle. There is one problem of
LSM330DLC
after
reflow solder.
The
LSM330DLC
has offset to detect
the angle from the vertical direction. The offset may be 0-7 degree, but they are still in good working condition.I made 1000 units of
LSM330DLC
based controller two times using
reflow solder
.
The ratio is about 15% that has offset problem. Others are good.
How to solve this problem?
Do you think the
LSM330DLC
are
affected by damp?The caution about
LSM330DLC is as follows.
1.After sealed bag is opened, devices that subjected to reflow solder must
a) mounted within: 168 hours at factory conditions <30
℃/60%RH
b) stored at <10
℃/60%RH
The
LSM330DLC
is not stored with above condition
I really didn't bake them befor
reflow solder.
Do you think the offset problem can be solved if I baked the
LSM330DLC
before
reflow solder?
Thanks
my email is: xmgatech@gmail.com