Skip to main content
Visitor II
December 12, 2023
Question

AcousticBF

  • December 12, 2023
  • 3 replies
  • 1860 views

Can the AcousticBF beamforming algorithm from FP-AUD-SMARTMIC1 algorithm be used on the entry-level kit of BlueCoin board (STEVAL-BCNCS01V1) to achieve audio acquisition at a sampling rate of 48kHz?

    This topic has been closed for replies.

    3 replies

    Technical Moderator
    December 12, 2023

    Hi @insist_66 ,

    Welcome to ST Community!

    The library AcousticBF can't work at 48KHz 

    insist_66Author
    Visitor II
    December 12, 2023

    The audio signal is obtained from the digital MEMSM Kefeng as a 1-bit PDM signal, which is then converted into a 16 bit PCM sample by a PDM to PCM conversion filter at 16 kHz. Using the AcousticBF algorithm in FP-AUD-SMARTMIC1, can a sampling rate of 48KHZ be achieved

    Technical Moderator
    December 13, 2023

    Hi @insist_66 ,

    I think there is a misunderstanding: the library only works up to 16KHz, both input and output.
    We don't have libraries or examples that from a 16KHz input signal would allow a 48KHz output signal.