Skip to main content
Visitor II
November 25, 2021
Question

After enabling the sensor hub I2C master bit in MASTER_CONFIG (1Ah) register of STEVAL-MKI182v2(ISM330DLC) I'm not able to read through ISM330DLC register for eg. 0x0f(WHO_AM_I).

  • November 25, 2021
  • 4 replies
  • 1778 views

STM NUCLEO-L4R5ZI-P is used to interface the  STEVAL-MKI182v2(ISM330DLC) .

    This topic has been closed for replies.

    4 replies

    Visitor II
    November 26, 2021

    Hi,

    Please consider this sentence:

    In order to enable the embedded functionalities of the ISM330DLC , the FUNC_EN bit of the CTRL10_C register has to be set to 1; after enabling the embedded functionalities, the MASTER_CONFIG register has to be used for the configuration of the I2C master interface.

    Not sure that, if the ISM330DLC is configured as I2C master, he cannot be treated as a slave from the application processor.

    See for example this example code on Github: https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lsm6dso_STdC/examples/lsm6dso_sensor_hub_lps22hh.c

    \Tom

    APatel.13Author
    Visitor II
    November 30, 2021

    Hi TBomb.1,

    Thank you for the reply.

    I followed the same process as per below link from Github: 

    https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lsm6dso_STdC/examples/lsm6dso_sensor_hub_lps22hh.c

    I tried to read device ID of LIS2MDL sensor and program get stuck inside below highlighted snippet of "ism330dlc_read_lis2mdl_cx" function and it seems that trigger flag never changed.

    static int32_t ism330dlc_read_lis2mdl_cx(void *ctx, uint8_t reg,

                        uint8_t *data, uint16_t len)

    {

    ism330dlc_sh_cfg_read_t sh_cfg_read;

    int32_t ret;

    ism330dlc_func_src1_t master_status;

    /* Disable accelerometer. */

    ret = ism330dlc_xl_data_rate_set(&ag_ctx, ISM330DLC_XL_ODR_OFF);

    if(ret != ISM330DLC_OK)

    return ISM330DLC_ERROR;

    /* Configure Sensor Hub to read LIS2MDL. */

    sh_cfg_read.slv_add = (LIS2MDL_I2C_ADD & 0xFEU) >> 1; /* 7bit I2C address */

    sh_cfg_read.slv_subadd = reg;

    sh_cfg_read.slv_len = len;

    ret = ism330dlc_sh_slv0_cfg_read(&ag_ctx, &sh_cfg_read);

    if(ret != ISM330DLC_OK)

    return ISM330DLC_ERROR;

    /* Configure number of slave connected to master I2C */

    ret = ism330dlc_sh_num_of_dev_connected_set(&ag_ctx, ISM330DLC_SLV_0);

    if(ret != ISM330DLC_OK)

    return ISM330DLC_ERROR;

    /* Enable I2C Master. */

    ret = ism330dlc_sh_master_set(&ag_ctx, PROPERTY_ENABLE);

    if(ret != ISM330DLC_OK)

    return ISM330DLC_ERROR;

    /* Enable accelerometer to trigger Sensor Hub operation. */

    ism330dlc_xl_data_rate_set(&ag_ctx, ISM330DLC_XL_ODR_12Hz5);

    if(ret != ISM330DLC_OK)

    return ISM330DLC_ERROR;

    /* Get XL raw data */

    ret = ism330dlc_acceleration_raw_get(&ag_ctx, &data_raw_acceleration.i16bit);

    if(ret != ISM330DLC_OK)

    return ISM330DLC_ERROR;

    /* Wait for XL(trigger) flag set. */

    do {

    HAL_Delay(20);

    ism330dlc_xl_flag_data_ready_get(&ag_ctx, &drdy);

    } while (!drdy);

    /* Wait Sensor Hub operation flag set. */

    do {

    HAL_Delay(20);

    ism330dlc_read_reg(&ag_ctx, ISM330DLC_FUNC_SRC1, (uint8_t *)&master_status, 1);

    } while (!master_status.sensorhub_end_op);

    /* Disable I2C master */

    ret = ism330dlc_sh_master_set(&ag_ctx, PROPERTY_DISABLE);

    if(ret != ISM330DLC_OK)

    return ISM330DLC_ERROR;

    /* Disable XL(trigger). */

    ret = ism330dlc_xl_data_rate_set(&ag_ctx, ISM330DLC_XL_ODR_OFF);

    if(ret != ISM330DLC_OK)

    return ISM330DLC_ERROR;

    /* Read SensorHub registers. */

    ret = ism330dlc_read_reg(&ag_ctx, ISM330DLC_SENSORHUB1_REG, data, len);

    if(ret != ISM330DLC_OK)

    return ISM330DLC_ERROR;

    return ret;

    }

    For your information :

    • Evaluation board used : NUCLEO-L4R5-ZI-P
    • ISM330DLC sensor used as a master I2C
    • LIS2MDL connected as I2C slave.

    Kindly suggest further how to read device id and data from LIS2MDL.

    regards,

    Ankur Patel

    Visitor II
    November 23, 2022

    @APatel.13 Hi, I am currently having the same problem that I replaced a LSM6DSL ( connected via SDx, SCx to a LIS3MDL compass ) with a ISM330DLC. But the sensorhub communication now does not work anymore. After starting a transfer by reenableing the Accelerometer the SENSORHUB_END_OP Bit in the FUNC_SRC1 register stays 0.

    I measured the SDx and SCx pins and they remain at 1.8V at all times.

    How did you solve this problem?

    Visitor II
    November 24, 2022

    @Eleon BORLINI

    Hi, is there any example on how to use the sensor-hub functionality of the ISM330DLC specifically? The examples for LSM6DSL don't seem to work. I guess it has something to do with the fact, that ISM330DLC has the additional operation Modes 3 & 4 which LSM6DSL did not have which also use the SDx and SCx pins but I did not enable these modes.

    Thanks