AIS2DW12 FF Int detect problems
Hello ,
I'm using an STM32U575 with an I2C connection to the AIS2DW12 accelerometer. The goal is to generate an interrupt when a free-fall event is detected. I followed the instructions provided in the datasheet (AN5326 - AIS2DW12 ultralow-power 3-axis accelerometer for automotive applications, STMicroelectronics).

I created a function to initialize the device using the specified register values, but no interrupt is detected. There are no hardware issues—when I force the INT1 pin to a high level, the MCU correctly enters the interrupt function. Later, I found a GitHub example for free-fall detection that doesn’t use interrupts. I still imported that code block into my project as an additional initialization function :
void AIS2DW12_FallDetection_Init(void) {
Ais2dw_ctx.write_reg = platform_ASW12_write;
Ais2dw_ctx.read_reg = platform_ASW12_read;
Ais2dw_ctx.mdelay = platform_ASW12_delay;
Ais2dw_ctx.handle = &hi2c3;
uint8_t whoamI, rst;
ais2dw12_reg_t int_route;
ais2dw12_device_id_get(&Ais2dw_ctx, &whoamI);
if (whoamI != AIS2DW12_ID)
while (1) {
/* manage here device not found */
}
/* Restore default configuration */
ais2dw12_reset_set(&Ais2dw_ctx, PROPERTY_ENABLE);
do {
ais2dw12_reset_get(&Ais2dw_ctx, &rst);
} while (rst);
/* Configure power mode */
ais2dw12_power_mode_set(&Ais2dw_ctx, AIS2DW12_PWR_MD_4);
/* Set Output Data Rate */
ais2dw12_data_rate_set(&Ais2dw_ctx, AIS2DW12_XL_ODR_100Hz);
/* Set full scale to 2 g */
ais2dw12_full_scale_set(&Ais2dw_ctx, AIS2DW12_2g);
/* Configure Free Fall duration and samples count */
ais2dw12_ff_dur_set(&Ais2dw_ctx, 0x06);
ais2dw12_ff_threshold_set(&Ais2dw_ctx, AIS2DW12_FF_TSH_10LSb_FS2g);
/* Enable free fall interrupt */
ais2dw12_pin_int1_route_get(&Ais2dw_ctx, &int_route.ctrl4_int1);
int_route.ctrl4_int1.int1_ff = PROPERTY_ENABLE;
ais2dw12_pin_int1_route_set(&Ais2dw_ctx, &int_route.ctrl4_int1);
/* Set latched interrupt */
ais2dw12_int_notification_set(&Ais2dw_ctx, AIS2DW12_INT_LATCHED);
}
In main function i've inserted this part:
int checkevent(void){
Ais2dw_ctx.write_reg = platform_ASW12_write;
Ais2dw_ctx.read_reg = platform_ASW12_read;
Ais2dw_ctx.mdelay = platform_ASW12_delay;
Ais2dw_ctx.handle = &hi2c3;
/* Check Free Fall events */
ais2dw12_all_sources_t src;
ais2dw12_all_sources_get(&Ais2dw_ctx, &src);
if ((src.all_int_src.ff_ia) || (src.status_dup.ff_ia) || (src.wake_up_src.ff_ia)) {
return 1;
}
return 0;
}
This code is taken from https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/ais2dw12_STdC/examples/ais2dw12_free_fall.c
Even with this method, the return value never changes to 1, despite aggressively moving the device. I’m using the STEVAL-MKI206V1 evaluation board. Do you have any suggestions to resolve this?
Thanks