Algobuilder flexible number of properties
Hi!
I am using Algobuilder and I tried to use a flexible number of properties (like for example in the "Graph"). Although undocumented, I saw in the library for the display that there are <DisplayDependency> and <DisplayCondition> tags. I tried to use them in a custom block, but unfortunately the user interface is not automatically updated when changing the number and the input fields for the properties do not appear.
It is working if I set a value and reload the entire functin block design or the library in algobuilder.
Is this a bug or is this feature simply not supported by custom made blocks?
Best wishes,
Dominik