Algobuilder With Sensor Hub
Hello,
I am trying to integrate the magnetic sensor data for the sensor_fusion_9x demo. I am using the F401RE+1A3+LSM6DSO16IS and when I leave the jumpers as standard I get no mag and the demo runs. I obviously get no mag data since the sensor hub is not being jumped in. When I change jumpers the to allow the IMU to act as a sensor hub then the device can connect but there is no option to start and i get no data at all. I did make sure to add the shub.ucf data to the demo.ucf so that I was initing the sensor and hub. At this point I dont know what I am doing wrong but the only thing i can think of is that the MCU software from algo builder cant find the sensors and it is blocking. Any help would be great.