Skip to main content
Visitor II
October 2, 2024
Question

Anti-alias IIS2DLPC

  • October 2, 2024
  • 1 reply
  • 545 views

I am trying to configure the IIS2DLPC for anti-aliasing as indicated by figure 3 section 3.4 of an5201.

AquaKnott_0-1727894408202.png

I am seeing frequency folding in the spectrum. I am playing a 300 and 500 Hz sine wave alternately on a sound table to vibrate the sensor. Each tone plays for 1.5s then switches frequency.

AquaKnott_2-1727896501799.png

I had the IIS2DLPC configured for, High Performance, 1600Hz ODR, and Band Width ORD/4 or 400Hz. I was expecting the 500Hz to be strongly attenuated. Is my understanding of how the anti-aliasing filter works, or my setup incorrect?

Here is the config code

 

 status = iis2dlpc_power_mode_set(&iis2dlpcctx, iis2dlpc_mode_t::IIS2DLPC_HIGH_PERFORMANCE); //IIS2DLPC_HIGH_PERFORMANCE_LOW_NOISE);
 report(status);

 status = iis2dlpc_data_rate_set(&iis2dlpcctx, iis2dlpc_odr_t::IIS2DLPC_XL_ODR_1k6Hz);//iis2dlpc_odr_t::IIS2DLPC_XL_ODR_12Hz5);//iis2dlpc_odr_t::IIS2DLPC_XL_ODR_1k6Hz);
 report(status);

 status = iis2dlpc_filter_bandwidth_set(&iis2dlpcctx, iis2dlpc_bw_filt_t::IIS2DLPC_ODR_DIV_4);
 report(status);

 // Set scale 2g/4g/8g/16g
 status = iis2dlpc_full_scale_set(&iis2dlpcctx, iis2dlpc_fs_t::IIS2DLPC_8g);
 report(status);

 

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    November 8, 2024

    Hi @AquaKnott ,

    what is the amplitude of the input signal? and what are the units of measurement of your plot?

     

    Thanks