AppMEMS#6b: The X-CUBE-MEMS1 libraries in detail - MotionAR functions
--- More detail about MotionAR library ---
The library is based on accelerometer data only, and requires a data sampling frequency of 16 Hz., and can to distinguish among the following activities: stationary, walking, fast walking, jogging, biking, driving.
The central function that performs the activity recognition is this one:
void MotionAR_Update (MAC_input_t *data_in, MAR_output_t *data_out, long int
timestamp)
*data_in parameter is a pointer to a structure with input data, *data_out parameter is a pointer to enum with the items described in the previous post and timestamp variable is a relative time for actual sample in ms.
See below the detailed output of the activity recognition of MotionAR algorithm! �?�