ASM330 SPI robustness
We are planning to use ASM330LHH at a distance of about 1m from the MCU to which it will interface for supplying the gyro data in an automotive application. SPI will run at around 1MHz. Can we interface directly through SPI, or should we integrate the sensor with anoother MCU and transmit the data to the main MCU over CAN? Are there any chances of data corruption over SPI due to EMI etc? Should we use any special wiring?