Skip to main content
Visitor II
November 3, 2024
Question

ASM330LHB performance?

  • November 3, 2024
  • 1 reply
  • 560 views

Hello,

ASM330LHB 6-axis sensor, can it reach 0.001g?

ASM330LHB 6-axis sensor that can reach 0.001g? how high can it reach?

Which 6-axis sensor is more accurate?

Can they both output angles?

 

This post has been translated from Chinese to comply with the ST Community guidelines.

 
 
    This topic has been closed for replies.

    1 reply

    Technical Moderator
    November 8, 2024

    Hi @1232 ,

    The maximum value that the sensor can reach and also the accuracy depend on the full scale you set according to datasheet:

    FedericaBossi_0-1731073939188.png

    If you want to reach higher g you can look at LSM6DSV32X that has a maximum full scale of 32g, but not that it is not for ASIL B automotive applications.

    Can they both output angles? Yes.