Skip to main content
Visitor II
December 15, 2025
Solved

ASM330LHHX : RES pin

  • December 15, 2025
  • 2 replies
  • 135 views

Hi 

What is the function of the RES pins on the ASM330LHHX?
The datasheet indicates: “Connect to VDDIO or GND.”
Is there a preferred connection?
Can I add a 4.7 kΩ pull-up or pull-down resistor?

BR

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    I suspect a typo and that instead of the ASM330LHHX, the ASM330LHH was actually meant, which has two pins labelled RES.

    If this is correct, then pins 2 and 3 are REServed pins that must be connected to a static potential so that these inputs do not pick up interference signals. The static potential can be achieved most cost-effectively with a fixed connection using a wire to GND or VDDIO, but of course also with pull-up resistors.

    Regards
    /Peter

    2 replies

    Super User
    December 15, 2025

    What pin? I do not see any pins labeled RES in the datasheet.

    TDK_0-1765824728261.png

     

    RES means reserved in this context. Typically this means the pin has some internal use during testing/development which is not intended or published to the user.

    Technical Moderator
    December 15, 2025

    I suspect a typo and that instead of the ASM330LHHX, the ASM330LHH was actually meant, which has two pins labelled RES.

    If this is correct, then pins 2 and 3 are REServed pins that must be connected to a static potential so that these inputs do not pick up interference signals. The static potential can be achieved most cost-effectively with a fixed connection using a wire to GND or VDDIO, but of course also with pull-up resistors.

    Regards
    /Peter

    Gilles_FRAuthor
    Visitor II
    December 16, 2025

    Hi
    Thanks

    it was about the two pins labelled RES.
    BR