Skip to main content
Visitor II
December 12, 2023
Question

BlueCoin入门套件

  • December 12, 2023
  • 2 replies
  • 965 views

BlueCoin入门套件使用波束形成算法时,采样率能达到多少啊

 

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    December 12, 2023

    Hi @insist_66 ,

    The BlueCoin can work at a maximum of 16kHz.

    insist_66Author
    Visitor II
    December 12, 2023

    The audio signal is obtained from the digital MEMSM Kefeng as a 1-bit PDM signal, which is then converted into a 16 bit PCM sample by a PDM to PCM conversion filter at 16 kHz. Using the AcousticBF algorithm in FP-AUD-SMARTMIC1, can a sampling rate of 48KHZ be achieved

    Technical Moderator
    December 14, 2023

    Hi @insist_66 ,

    Unfortunately this is not possible: the library only works up to 16KHz, both input and output.
    We don't have libraries or examples that from a 16KHz input signal would allow a 48KHz output signal.