Skip to main content
Visitor II
December 20, 2017
Question

BlueNRG-MS

  • December 20, 2017
  • 0 replies
  • 722 views
Posted on December 20, 2017 at 09:44

Hello,

I am working with the SPBTLE-RF module interfaced with a freescale IMX6 microcontroller.

Right now I am porting the Beacon example code to my platform (WEC2013) and I am facing an issue with the SPI communication. When sending the Header (0x0A00000000 or 0x0B00000000), the reply from the component is 0x047F000600.

My guess is that I am pulling the Chip Select too early. I have 40 microseconds between the moment when I pull down the CS and the moment of the first clock tick (cf. 'signaux I2C2-00002--00002.png' attached below, deltaX=40us).

I also attach to this post 2 others screenshots of the exchange corresponding to the header. You will see that the answer from the module SPBTLE-RF starts with 0x04 instead of 0x02.

Thanks for your help.

Maxime

#ble #bluenrg-ms #spbtle-rf #spi
    This topic has been closed for replies.