Skip to main content
Visitor II
June 6, 2019
Question

Bluetooth communication issues with unicleo GUI and sensorTile

  • June 6, 2019
  • 13 replies
  • 4084 views

Hi,

I'm facing with a issue on unicleo gui and sensorTile sensor (with ALLMEMS1 and ALLMEMS2 librairies).

I dont know why, but since few day i can pair and connect my sensor tile with bluetooth on my laptop (W10) but unicleo doesn't show the normal interface with sensor picture and librairies selection.

i try to update my bluetooth driver, update gui to 1.8, uninstal/install all driver and soft but same pb!

Is anybody encountered the same pb, and have a workaround?

For finish, sensorTile work fine with Android STBLE app!

0690X000008iKybQAE.jpg

thanks

    This topic has been closed for replies.

    13 replies

    Visitor II
    May 28, 2020

    Hi Daniel,

    Try do download this utility https://live.sysinternals.com/Dbgview.exe this application can catch debug messages from applications. Run this application and then run Unicleo-GUI and then sent the log to me.

    Visitor II
    September 18, 2020

    0693W000004GPJGQA4.pngHi louda.marian,

    I have the same problem of DMari.1 (Unicleo-GUI not recognize the evaluation board STEVAL-MKSBOX1V1); in the following, I attach the screenshot of Dbgview output.

    Please help me!

    Thanks a lot,

    Giovanni

    Visitor II
    September 21, 2020

    Hi Giovanni,

    There are two necessary conditions for the device to be displayed in Unicleo. First one, the device must be paired in windows. Second one, the device must contain Generic Access service( if you use any from FWs from ST it should be valid). In your case there are no any error messages in debug output and if you do not see any device it means that no device was found. If you have the device already paired, try to unpair and pair again the device (pin 123456). BLE device list is refreshed only during start of application, so you have to restart the application to see changes. I am not able to repeat the situation that the device is visible in a list of paired devices in windows and is not visible in Unicleo.

    Best Regards,

    Marian