Can I set LIS2DW12 ODR to 1600Hz in High Performance mode with a BW of ODR/2?
Currently I am using LIS2DW12 in my project with ODR set to 1600Hz in High performance mode. Reading the datasheet I found that the maximum bandwidth for this ODR ir 400Hz. I want to understand why tye maximum bandwidth for this setting is 400Hz and not 800Hz. I also want to know if it is possible to set the bandwidth to 800Hz with ODR set to 1600Hz.